Status LED - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

The green Status LED is located to the right of the heartbeat (BEAT) LED. This LED provides a central processing unit (CPU) machine status check, and remains lit whenever the FX30E/FX60E is powered. If the Status LED does not light while power is applied, contact your technical support representative for assistance.