Checking the status LEDs - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
Language
English

When power is applied, the green LED labeled Status is lit. This LED status indicates that the system is normal and power is applied. Once the FX30E/FX60E boots, the yellow BEAT (heartbeat) LED begins to blink, with a typical rate of about one blink per second. Blinking should begin within 30 seconds after power is applied.

If, after applying power, the STATUS LED goes out, or the BEAT LED comes on steady and stays lit for longer than 2 minutes, contact your technical support representative for assistance. See also Using status LEDs.