Serial ports - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

The FX30E/FX60E has two serial ports (Figure 1). Each port has a Universal Asynchronous Receive Transmit (UART) capable of operating up to 115,200 baud. The left port is an RS-232 port that requires a DB-9 male plug connector. The right port is a non-isolated RS-485 port that uses two wires with a shield connection and a screw-terminal connector plug.

Note: A green receive LED and yellow transmit LED are provided for each serial port. These LEDs are located on the bottom board opposite of the serial connectors (Figure 7). The LEDs are labeled on the board (COM1, COM2) and are not visible with the cover on.