Repair information - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

Servicing the FX30E/FX60E may call for replacement parts.

Non-replaceable Parts

Other than the parts listed in the Standard Replacement Parts section, no serviceable components are on the base assembly.

Memory

Any addition, modification, or replacement of memory components requires software configuration changes and is not field upgradeable. For additional information on modifying the memory capacity of the FX30E/FX60E, consult your local sales representative.

Fuse

The FX30E/FX60E contains a non-user replaceable fuse soldered on the circuit board. This fuse provides protection from internal shorts or connection to incorrect power supplies. If the fuse circuitry is suspect, contact your technical support representative for assistance.