Removing and replacing the cover - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
Language
English

The FX30E/FX60E cover is removable. You must remove the FX30E/FX60E cover to connect the optional battery on a new unit, to replace the optional battery on an existing unit, or to install any optional communication cards. The cover snaps onto the base with four plastic tabs (two on each end). To remove the cover, press in the four tabs on both ends of the unit and lift off the cover.

Note: If accessory modules are plugged into the FX30E/FX60E, you may need to slide them away from the unit to get to the cover tabs.

To replace the cover, position it so the cutout area for the communication ports is correct, then push inward to snap in place.