Reassembling the Controller - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller
FX30E/FX60E Supervisory Controllers Installation Instructions
- Product
- Controls > Supervisory Controls > FX Supervisory Controller
- Document type
- Installation Guide
- Document number
- Part No. 24-10174-115
- Document revision
- E
- Revision date
- 2019-03-22
Procedure
-
Carefully replace the processor module board onto the 50-pin connector, with its corner mounting holes aligned on the four lower standoffs. Press down on the connector to fully seat the board.
-
Refasten the four metal hex standoffs by hand tightening with a 1/4 in. (7 mm) nut driver.
-
Replace the shield back onto the unit. Carefully ease the shield over the port side first and then spring it down over the other side. Make sure that the shield’s corner holes align with the metal standoffs.
-
With a Phillips head screwdriver, refasten the four screws that secure the shield to the standoffs.
-
Replace the plastic cover onto the unit.