Providing power and connectivity - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

Perform the initial startup of an FX30E/FX60E in your office before physically mounting it in place at a job site.

After you complete the commissioning process, mount and wire the FX30E/FX60E at the job site, making permanent mounting and wiring connections.

For this initial Ethernet connection, you can use one of the following:
  • a crossover cable connected directly between your computer and the FX30E/FX60E
  • a standard Local Area Network (LAN) connection in which your computer and the FX30E/FX60E are physically connected to the same Ethernet hub or switch