About this task
An FX30E/FX60E Series controller is shipped with the following Platform Daemon (Administrator) credentials:
User Name: jci
Password: Contact your local Johnson Controls representative for the default password.
Initially, you use these default credentials to open a platform connection (log in) to the FX30E/FX60E. Like the factory-assigned IP address, default credentials are intended to be temporary. Change these credentials to be something unique, and guard them closely.
Procedure
- Start the FX Workbench application.
- On the File Menu, click Open Remote Station. When prompted, enter the Remote Site Address (for example, 192.168.1.149), Remote Username (jci), and Remote Password. Click OK. When the Authentication dialog box appears, enter the Username (admin), leave the password field empty, and click OK.
- On the Tools menu, click Change Remote Platform Login Credentials. In the Change Remote Login Credentials dialog box, fill in the Username, Password, and Confirm Password fields, then click OK. The next time you log into the FX30E/FX60E, use these new credentials.