Powerup and initial checkout - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
Language
English

About this task

Ensure that power wiring to the transformer is complete before you proceed.

After you have completed all mounting and wiring steps:

Procedure

  1. Do one of the following:
    • Insert the power plug into either the 24 VAC/DC power module, or if using a wall adapter, the FX30E/FX60E.

    • Energize the 120–240 VAC circuit wired to the module, if using the line voltage power supply module.
  2. Apply power.
    Important: Do not connect both the wall power module and the DIN rail power modules at the same time, or equipment damage will result, or a power outage may go unrecognized.