Option cards - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
Language
English
The FX30E/FX60E has two options slots for custom option cards designed for use with the FX30E/FX60E. Each slot has a 30-pin connector on the FX30E/FX60E base unit.
CAUTION:
  • Risk of Property Damage.
  • Do not apply power to the system before checking all wiring connections. Short circuited or improperly connected wires may result in permanent damage to the equipment.
CAUTION:
  • Risque dégâts matériels.
  • Ne pas mettre le système sous tension avant d'avoir vérifié tous les raccords de câblage. Des fils formant un court-circuit ou connectés de façon incorrecte risquent d'endommager irrémédiablement l'équipement.
Important: Power to the controller must be off when installing or removing option cards or damage will occur.
Important: Be careful to plug an option card into the connector properly with its pins properly aligned.

Option cards typically provide additional communication capabilities, such as those listed in Table 2. For a list of supported COM port and slot assignments for the option cards, see Table 3.