NiagaraAX software installation - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

As shipped from the factory, the FX30E/FX60E is preconfigured with a Niagara build, a license, and Johnson Controls® specific Java® Archive (JAR) files. With these components in place, you only need to change login credentials and IP settings (per network requirements) when setting up the FX30E/FX60E. This section provides step-by-step instructions for these tasks.

To set up an FX30E/FX60E (and to upgrade to a newer Niagara build at a later date), use the Commissioning Wizard in the Platform/Platform Administration view.

Note: If you plan to update the JAR files with patches at a later date, use the Driver Upgrade Tool Commissioning Wizard or Software Manager in the Platform view. If you are changing login credentials, use the Change Remote Login Credentials menu item.