Physical mounting - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

The following information applies to the physical mounting of the FX30E/FX60E.

  • You do not need to remove the cover before mounting.
  • Mount the FX30E/FX60E in any orientation.
  • Mount the unit on a 35-mm wide DIN rail (recommended). The FX30E/FX60E unit base and its accessories have molded DIN rail slots and locking clips. Mounting these components on a DIN rail ensures accurate alignment of connectors between all modules.
  • If DIN rail mounting is impractical, use screws in mounting tabs on the FX30E/FX60E and in any end-connected accessory (power module, NDIO module). See Figure 2 for tab dimensions.