DIN rail mounting instructions - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
Language
English

About this task

Procedure

  1. Securely install the DIN rail using at least two screws near both ends of the rail.
  2. Position the FX30E/FX60E on the rail, then tilt it to hook the DIN rail tabs over one edge of the DIN rail (Figure 3).
  3. Use a screwdriver to pry down the plastic locking clip, and push the FX30E/FX60E down and in, which forces the locking clip to snap over the edge of the DIN rail.
  4. Mount the accessory modules (NDIO modules and power module) onto the DIN rail in the same manner (Figure 5). See Table 1 for quantities allowed.
  5. Slide the accessory along the DIN rail to connect its 20-position plug into the FX30E/FX60E.
  6. Repeat these instructions for all accessories, until all are mounted on the DIN rail and firmly connected to each other. For an example, see Figure 4.
    To keep the final assembly together, secure the assembly at both ends with DIN rail end-clips. This action also prevents the assembly from sliding on the DIN rail. See Figure 4.