Mounting - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

Mount the FX30E/FX60E in a location that allows clearance for wiring, servicing, and module removal.

Follow these recommendations and precautions when mounting and installing the unit.

  • Use this controller for indoor use only. Do not expose the unit to ambient conditions outside the range of 0ºC to 50ºC (32ºF to 122ºF) and relative humidity outside the range of noncondensing 5% to 95% (Pollution Degree 3).

  • Supply voltage requirements are as follows:
    • Allowable voltage fluctuation to -15%, +10%, Temporary overvoltages +/- 15%
    • Transient overvoltages: Overvoltage Category 2
  • For a controller mounted inside an enclosure, ensure that the enclosure is designed to keep the unit within its required operating range (considering a 20-watt dissipation by the controller). This enclosure is especially important if the controller is mounted inside an enclosure with other heat producing equipment.

  • Do not mount the unit:
    • in an area where excessive moisture, corrosive fumes, or explosive vapors are present
    • where vibration or shock is likely to occur
    • in a location subject to electrical noise. This includes the proximity of large electrical contactors, electrical machinery, welding equipment, variable frequency drives, and spark igniters.