Static discharge precautions - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

Static charges produce voltages high enough to damage electronic components. The microprocessors and associated circuitry within an FX30E/FX60E are sensitive to static discharge.

Important: Work in a static-free area. Discharge any static electricity you may have accumulated. Discharge static electricity by touching a known, securely grounded object. Do not handle the Printed Circuit Board (PCB) without proper protection against static discharge. Use a wrist strap when handling PCBs. Secure the wrist strap clamp to earth ground.