Safety precautions - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
The following information relates to the installation and startup of the FX30E/FX60E.
Warning:
  • Risk of Electric Shock
  • Disconnect the power supply before making electrical connections. Contact with components carrying hazardous voltage can cause electric shock and may result in severe personal injury or death.
Warning:
  • AVERTISSEMENT
  • Risque de décharge électrique. Débrancher l'alimentation avant de réaliser tout branchement électrique. Tout contact avec des composants conducteurs de tensions dangereuses risque d'entraîner une décharge électrique et de provoquer des blessures graves, voire mortelles.
Important: Use copper conductors only. Make all wiring connections in accordance with local, national, and regional regulations. Do not exceed the FX30E/FX60E electrical ratings.
Important: Do not install or use the FX30E/FX60E in or near environments where corrosive substances or vapor could be present. Exposure of the FX30E/FX60E to corrosive environments may damage the device's internal components, and will void the warranty.
Important: Use this FX30E/FX60E only as an operating control. Where failure or malfunction of the FX30E/FX60E could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed in the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the FX30E/FX60E.