Expansion options - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
The FX30E/FX60E provides for field-installable expansion with two options:
  • Option Cards: these are installed on connectors inside the FX30E/FX60E base unit. See Option cards.
  • Accessory Modules: these are chained onto the FX30E/FX60E’s 20-pin connector. See Accessories.