Board layout - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

See Figure 7 for the location of LEDs, option slots, and other features of the FX30E/FX60E. See Figure 1 for a side view of communication ports and other features. The FX30E/FX60E ships with onboard static RAM (SRAM) that can provide station backup during power loss, and also has two open option card slots for a variety of available option cards.

Note: An optional NiMH battery pack is included, but not connected. For connection instructions, see Backup Configurations.