Enabling battery only backup service - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

If a station is not compatible with SRAM support and you want to use the optional backup battery instead of the onboard SRAM, connect the optional NiMH battery pack to the FX30E or FX60E.

In the station’s DataRecovery-Service, set the Service Enabled property to false. In the station’s PlatformServices, make sure the Battery Present property is true.