Accessories - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22

The FX30E/FX60E has a 20-pin, right-angle, Euro-DIN connector that accepts accessory modules. The connector provides power and signal lines to any connected modules. The connector is located on the end of the FX30E/FX60E opposite the option cards.

Important: Turn off power to the FX30E/FX60E before inserting or unplugging accessory modules. Wait for the LED activity to stop (all LEDs off).
CAUTION:
  • Risk of Property Damage.
  • Do not apply power to the system before checking all wiring connections. Short circuited or improperly connected wires may result in permanent damage to the equipment.
CAUTION:
  • Mise en Garde: Risque dégâts matériels.
  • Ne pas mettre le système sous tension avant d'avoir vérifié tous les raccords de câblage. Des fils formant un court-circuit ou connectés de façon incorrecte risquent d'endommager irrémédiablement l'équipement.

Each accessory module has a DIN-mount base, and typically provides two 20-pin connectors that allow you to chain multiple accessories (see DIN rail mounting instructions). Table 1 lists the currently available modules.