Wiring considerations and guidelines - Facility Explorer - Part No. 24-10325-29 - FX-ZFR1811-1 - FX-ZFR1811-0 - FX-ZFRCBL-0 - FX-ZFRRPT-0 - Bulb controller - FX-ZFR1811 Wireless Field Bus Router

FX-ZFR1811 Wireless Field Bus Router Installation Instructions

Product
Network and Communications > Wireless Devices > FX-ZFR1811 Wireless Field Bus Router
Document type
Installation Guide
Document number
Part No. 24-10325-29
Document revision
C
Revision date
22/03/2019
Important: Do not connect supply power to the FX-ZFR1811 Router before finishing wiring and checking all wiring connections. Short circuits or improperly connected wires may result in permanent damage to the Router.
Important: Use copper conductors only. Make all wiring in accordance with local, national, and regional regulations. The FX-ZFR1811 Router is a low-voltage (less than 30 VAC) device. Do not exceed the FX-ZFR1811 Router’s electrical ratings.
Important: Prevent any static electric discharge to the FX-ZFR1811 Router. Static electric discharge can damage the FX-ZFR1811 Router and void any warranties.
Important: Do not connect the FX-ZFR1811 Router to the power supply before setting the PAN OFFSET switches.

Wiring with an FX-PCG or FX-PCA Series Field Controller

Connect the FX-ZFR1811 Router to the field controller as shown in Table 1. This connection provides both power and communication to the FX-ZFR1811 Router.

Note: When using a field controller in a wireless field bus network, ensure that the DIP switch for Address 128 is set to the ON position.