LED status - Facility Explorer - Part No. 24-10325-29 - FX-ZFR1811-1 - FX-ZFR1811-0 - FX-ZFRCBL-0 - FX-ZFRRPT-0 - Bulb controller - FX-ZFR1811 Wireless Field Bus Router

FX-ZFR1811 Wireless Field Bus Router Installation Instructions

Product
Network and Communications > Wireless Devices > FX-ZFR1811 Wireless Field Bus Router
Document number
Part No. 24-10325-29
Document revision
C
Revision date
22/03/2019
Table 1. FX-ZFR1811 router status LED

Name

Visual Indication of:

Descriptions

General Operation

Normal

operation

OFF Steady = No power (or normal operation for more than 2 hours).

OFF Steady with 1 Flash every 10 seconds = FX-ZFR1811 Router is not a member of a wireless network, invalid PAN OFFSET setting, no FX-ZFR1810 Coordinators or FX-ZFR1811 Routers in area.

ON Steady with Signal Strength displayed once every 10 seconds = FX-ZFR1811 Router is a member of a wireless network.

OFF Steady with Signal Strength displayed once every 10 seconds = Wireless network is actively communicating, but FX-ZFR1810 Coordinator cannot be reached (for example, coordinator lost power).

Signal Strength Indication 1

Wireless signal

strength

3 Flashes - Excellent

2 Flashes - Good

1 Flash - Weak

OFF for 3 seconds - None

Network Reform

Operation

during network

reform

Rapid Flashes for 5 minutes = rapid flashes occur for up to 5 minutes:

  • when the Reform Network option is initiated to the network, the FX-ZFR1811 Router disconnects itself from the network
  • when the PAN OFFSET is changed on the FX-ZFR1811 Router
  • when the PAN OFFSET is changed on the FX-ZFR1811 Router after it has already joined another PAN
  • when the Channel Mask in the FX-ZFR1810 is changed from CCT

Network Ping

Wireless node

function in the

network

Network pings provide a means of physically locating connected devices. There are two

methods with different use cases:

1) Use FX-ZFR Checkout Tool (FX-ZCT) to ping an address. This LED on the connected FX-ZFR1811

to blink, indicating the device mapped to that specific MS/TP address

2) Press the Occupancy pushbutton on a FX-WRZ Network Sensor. This causes the blinking

response on the FX-ZFR1811 connected to the paired device. This can be used to validate

switch settings on the sensor during installation.

1 The Signal Strength LEDs on all the FX-ZFR1811 Routers in a network extinguish after approximately 2 hours or normal operation, making the FX-ZFR1811 less distracting when installed in an open area. To re-enable the FX-ZFR1811 LEDs for troubleshooting purposes, perform a scan using the FX-ZCT or push the Status Push Button on the FX-ZFR1810 Coordinator.