Installation - Facility Explorer - Part No. 24-10325-29 - FX-ZFR1811-0 - FX-ZFR1811-1 - FX-ZFRCBL-0 - FX-ZFRRPT-0 - Bulb controller - FX-ZFR1811 Wireless Field Bus Router

FX-ZFR1811 Wireless Field Bus Router Installation Instructions

Product
Network and Communications > Wireless Devices > FX-ZFR1811 Wireless Field Bus Router
Document type
Installation Guide
Document number
Part No. 24-10325-29
Document revision
C
Revision date
22/03/2019
Important: Before installing the FX-ZFR1811 Router in plenum applications, verify acceptance of exposed plastic materials in plenum areas with the local building authority. Building codes for plenum requirements vary by location. Some local building authorities accept compliance to UL 1995, Heating and Cooling Equipment, whereas others use different acceptance criteria.

Follow these guidelines when installing an FX-ZFR1811 Router:

  • Transport the FX-ZFR1811 Router in the original container to minimize vibration and shock damage.

  • Verify that one 1/2 in. trade size Electrical Mechanical Tubing (EMT) connector is shipped with the FX-ZFR1811 Router.

  • Do not drop the FX-ZFR1811 Router or subject it to physical shock.