Mounting the FX-WRZ Handheld Temperature Room Sensor - Facility Explorer - Part No. 24-10724-19 - FX-WRZTTB00-5 - Bulb controller - FX-WRZTTB00-5 Handheld Temperature Room Sensor

FX-WRZTTB00-5 Handheld Temperature Room Sensor Installation Instructions

Product
Sensors and Meters > Room Sensor > FX-WRZTTB00-5 Handheld Temperature Room Sensor
Document number
Part No. 24-10724-19
Document revision
E
Revision date
2019-04-05

About this task

The FX-WRZ Handheld Temperature Room Sensor needs to be securely mounted with its tether cord to an object that remains within the room. Mounting the sensor to the head wall system with the tether cord is the preferred method. Actual installation of the tether cord varies based on room parameters, but we recommend using a security anchor from a Johnson Controls approved vendor such as Tufnut (www.tufnut.com). Tufnut also offers anchor plates as well as security screws that can be used to secure a looped and crimped end of the tethered cord.