Temporary storage of the room sensor - Facility Explorer - Part No. 24-10724-19 - FX-WRZTTB00-5 - Bulb controller - FX-WRZTTB00-5 Handheld Temperature Room Sensor

FX-WRZTTB00-5 Handheld Temperature Room Sensor Installation Instructions

Product
Sensors and Meters > Room Sensor > FX-WRZTTB00-5 Handheld Temperature Room Sensor
Document type
Installation Guide
Document number
Part No. 24-10724-19
Document revision
E
Revision date
05/04/2019

When the sensor must be temporarily stored away from the bed, we recommend locating the temperature room sensor on the head wall system near where the tethered cable is anchored. This can be accomplished with two different methods.

Hook storage

Secure a hook that can support the weight of the sensor on the wall (Figure 7). Place the opening of the loop of the tethered cable on the hook. You can purchase the hook from a hardware or office supply store.

Figure 1. Hook storage

Holder storage

Secure a holder that can support the weight of the sensor on a wall (Figure 8). Make sure the holder is the proper size (approximately 7-3/4 x 4-3/8 x 3-1/4 in. [19.6 x 10.7 x 8.2 cm]) and style to securely cradle the temperature room sensor. You can purchase the holder from a hardware or office supply store such as Office Depot (item 447534) or Office Max (item 20031877).

Figure 2. Sensor anchored to wall below holder