Testing signal strength - Facility Explorer - Part No. 24-10724-19 - FX-WRZTTB00-5 - Bulb controller - FX-WRZTTB00-5 Handheld Temperature Room Sensor

FX-WRZTTB00-5 Handheld Temperature Room Sensor Installation Instructions

Product
Sensors and Meters > Room Sensor > FX-WRZTTB00-5 Handheld Temperature Room Sensor
Document number
Part No. 24-10724-19
Document revision
E
Revision date
2019-04-05

Once the FX-WRZ sensor is communicating with the FX-ZFR or FX-ZFR Pro Series Router or FX-WRZ78xx Receiver, press and release the manual occupancy override button to display the signal strength.

Press and hold the manual occupancy override button on the FX-WRZ Handheld Temperature Room Sensor (Figure 1) for 5 seconds or more to place the sensor into Rapid Transmit Mode and initiate a signal strength test with the associated FX-ZFR or FX-ZFR Pro Series Router or FX-WRZ78xx Receiver.

See Rapid Transmit Mode for more information.

Table 1. FX-WRZ Sensor to FX-ZFR or FX-ZFR Pro Series Router or FX-WRZ78xx Receiver Wireless signal strength
Bars Signal Strength
3 Excellent: Sensor has joined network
2 Good: Sensor has joined network
1 Weak: Sensor has joined network
0 None: Sensor has not joined network

The signal strength is shown on the display on the face of the sensor (Figure 15).

Figure 1. Sensor LCD

Before installation, an optional FX-WRZSST-120 Wireless Sensing System Tool can be used with any FX-WRZ Handheld Temperature Room Sensor as a site survey tool, to determine potential locations for system devices and to determine the wireless signal strength between the system devices in the application.

Refer to the FX-WRZSST-120 Wireless Sensing System Tool Installation Instructions(Part No. 24-10563-71) for more information on testing signal strength. For additional location consideration details, refer to the following documents:

  • FX-ZFR Series Wireless Field Bus System Technical Bulletin (LIT-12011660)
  • FX-WRZ7860 One-to-One Wireless Sensing System Technical Bulletin (LIT-12011663)
  • WNC1800/FX-ZFR182x Pro Series Wireless Field Bus System Technical Bulletin (LIT-12012396)