Mesh mode - Facility Explorer - Part No. 24-10724-19 - FX-WRZTTB00-5 - Bulb controller - FX-WRZTTB00-5 Handheld Temperature Room Sensor

FX-WRZTTB00-5 Handheld Temperature Room Sensor Installation Instructions

Product
Sensors and Meters > Room Sensor > FX-WRZTTB00-5 Handheld Temperature Room Sensor
Document number
Part No. 24-10724-19
Document revision
E
Revision date
2019-04-05

You can add up to nine FX-WRZ Handheld Temperature Room Sensors per FX-PCA, FX-PCG, or FX-PCV in mesh mode.

The Zone DIP switches on the FX-WRZ Sensor relate to the Zone Netsensor (SA Bus device) address configured for the sensor in the Controller Configuration Tool (CCT). For example, if you set the Zone DIP switches to a value of 3 (that is, if DIP switch 1 and 2 are set to ON), you must use Zone Netsensor address 202 in the CCT. You can add up to nine FX-WRZ Sensors per controller. You can use any nine of the sixteen available Zone Netsensor address settings at a time.

The mesh mode of operation is intended for use with the FX-ZFR1800 Series or FX-WNC1800/ZFR182x Pro Series Wireless Field Bus Systems. The following table describes the Zone DIP switch settings for the wireless applications in mesh mode.

Table 1. Zone switch and SA bus settings when using multiple FX-WRZ sensors
Zone DIP switch ON Zone Netsensor (SA Bus Device) address setting
None (All OFF) 199
1 200
2 201
1 and 2 202
4 203
1 and 4 204
2 and 4 205
1, 2, and 4 206
8 207
1 and 8 208
2 and 8 209
1, 2, and 8 210
4 and 8 211
1, 4, and 8 212
2, 4, and 8 213
1, 2, 4, and 8 214
1 Use the one-to-one application DIP switch overlay in one-to-one mode, or the mesh application DIP switch overlay in mesh mode. The switch numbers described in this table refer to the numbers on the overlays.