Attaching the sensor to the hospital bed - Facility Explorer - Part No. 24-10724-19 - FX-WRZTTB00-5 - Bulb controller - FX-WRZTTB00-5 Handheld Temperature Room Sensor

FX-WRZTTB00-5 Handheld Temperature Room Sensor Installation Instructions

Product
Sensors and Meters > Room Sensor > FX-WRZTTB00-5 Handheld Temperature Room Sensor
Document type
Installation Guide
Document number
Part No. 24-10724-19
Document revision
E
Revision date
05/04/2019

About this task

You can attach the room sensor to the hospital bed in a number of ways. The first way is to wrap the tether cord around the hand rail a few times so it does not slide off of the bed, making sure that the patient has access to the sensor.

Another way is to attach a security clip to the cable near the sensor end and then clip the cable to the bed. Be sure to position the clip in a way that does not come undone or interfere with the position of the bed. You can purchase a security clip from a healthcare supply company such as Crest Healthcare Supply (www.cresthealthcare.com) or Ocelco Healthcare Equipment and Parts (www.ocelo.com).

Figure 1. Tether cable attached to bed