Special tools needed - Facility Explorer - Part No. 24-10724-19 - FX-WRZTTB00-5 - Bulb controller - FX-WRZTTB00-5 Handheld Temperature Room Sensor

FX-WRZTTB00-5 Handheld Temperature Room Sensor Installation Instructions

Product
Sensors and Meters > Room Sensor > FX-WRZTTB00-5 Handheld Temperature Room Sensor
Document type
Installation Guide
Document number
Part No. 24-10724-19
Document revision
E
Revision date
05/04/2019
  • 1/16 in. (1.6 mm) Allen wrench or Johnson Controls® T-4000-119 Allen-Head Adjustment Tool (order separately) for thetamper-resistant set screw that secures the transmitter to the mounting base
  • Coin for unlocking the sensor housing from the mounting base locking tab
  • Tool to crimp the aluminum sleeves to the tether cable
  • Wire cutter to cut the tether cable
  • Phillips screwdriver for accessing the battery holder