Dimensions - Facility Explorer - Part No. 24-10724-19 - FX-WRZTTB00-5 - Bulb controller - FX-WRZTTB00-5 Handheld Temperature Room Sensor

FX-WRZTTB00-5 Handheld Temperature Room Sensor Installation Instructions

Product
Sensors and Meters > Room Sensor > FX-WRZTTB00-5 Handheld Temperature Room Sensor
Document number
Part No. 24-10724-19
Document revision
E
Revision date
2019-04-05

See Figure 1 for dimensions and physical features of the FX-WRZ Handheld Temperature Room Sensor.

Figure 1. FX-WRZ Handheld Temperature Room Sensor - physical features and dimensions,in. (mm)