Installation - Facility Explorer - Part No. 24-10724-19 - FX-WRZTTB00-5 - Bulb controller - FX-WRZTTB00-5 Handheld Temperature Room Sensor

FX-WRZTTB00-5 Handheld Temperature Room Sensor Installation Instructions

Product
Sensors and Meters > Room Sensor > FX-WRZTTB00-5 Handheld Temperature Room Sensor
Document type
Installation Guide
Document number
Part No. 24-10724-19
Document revision
E
Revision date
05/04/2019

Follow these guidelines when installing theFX-WRZ Sensor:

  • Transport the sensor in the original container to minimize vibration and shock damage.
  • Verify that all the parts shipped with the sensor.
  • Do not drop the sensor or subject it to physical shock.
  • Do not attempt to remove or repair the circuit board from the sensor housing. Other than battery replacement, the sensor is not user-serviceable.