Commissioning procedure workflow - Facility Explorer - LIT-12011663 - Wireless Device - WRZ: Wireless Room Sensing System

FX-WRZ Series One-to-One Wireless Room Sensing System Technical Bulletin

Brand
Facility Explorer
Product name
WRZ: Wireless Room Sensing System
Document type
Technical Bulletin
Document number
LIT-12011663
Revision date
2019-04-04
Language
English

The procedure required to commission and configure a One-to-One wireless room sensing system can be performed in a variety of sequences. The job site and workflow dictate the order in which these procedures are performed. The following procedure order is a typical sequence.

To commission and configure a One-to-One Wireless Sensing system, you must perform the following procedures:

  • Install, commission, and configure the target FX-PC controller.
  • Commission/address and install the FX-WRZ7860 Receiver.
  • Connect the FX-WRZ7860 Receiver to the target controller.
  • Install and address the FX-WRZ Series Sensors.
  • Test the RF signal strength between the associated devices.
  • Test and confirm operation of the complete application.