Manual occupancy override button - Facility Explorer - LIT-12011663 - Wireless Device - WRZ: Wireless Room Sensing System

FX-WRZ Series One-to-One Wireless Room Sensing System Technical Bulletin

Brand
Facility Explorer
Product name
WRZ: Wireless Room Sensing System
Document type
Technical Bulletin
Document number
LIT-12011663
Revision date
2019-04-04
Language
English

Pressing the manual occupancy override button, which is located on the left side of the sensor, serves two main functions. First, it temporarily sets the space to an occupied state. Second, it checks the wireless signal strength of the sensor. The LED on the sensor flashes 3 times to indicate a strong signal, 2 times to indicate a good signal, or 1 time to indicate a marginal signal. For sensors with an LCD display, a number of bars on the display indicates wireless signal strength (3 bars for a strong signal, 2 bars for a good signal, or 1 bar for a marginal signal).

Note: Not all features shown on Figure 2 and Figure 3 are available on all models. See Table 2 for a list of features on each model.
Figure 1. FX-WRZ Series Sensor; LCD with occupancy sensor and setpoint adjustment dial, physical features and dimensions, in. (mm)