Introduction - Facility Explorer - LIT-12012253 - Server - FX Alarm Portal - FX Workbench - FX Server - 14.x

FX Supervisory Controller Family Software Products Release 14.x Installation Guide

Product
Building Automation Systems > Alarm Portals > FX Alarm Portal
Building Automation Systems > Graphics and Interfaces > FX Workbench
Building Automation Systems > Application Servers > FX Server
Document number
LIT-12012253
Version
14.x
Revision date
2023-03-07

Welcome to the FX Supervisory Controller Family software installation and configuration instructions. This document covers the initial software installation of the following products:

  • FX Workbench
  • FX Server

This document is meant for application engineers, system representatives, field installation and service technicians, and others performing control system installation.

This document does not cover the operation of Johnson Controls® customized versions of FX Workbench (FX Workbench Pro and FX Workbench) or NiagaraAX components. For more information on these versions and components, refer to the FX Workbench 14.x User Guide (LIT-12012256) or the Niagara User’s Guide located in docs\docUser folder of your FX Supervisory Software installation directory.

Note: The default installation directory for the FX Workbench User’s Guide is C:\JCI\FXWorkbench-#.#\jciStandards, where [#.#] is replaced by the revision level of the software.
Note: The default installation directory for the Niagara User’s Guide is C:\JCI\FXWorkbench-#.#\docs\ docUser, where [#.#] is replaced by the revision level of the software. However, you can specify a different installation directory during the installation process. Ensure you have the correct directory path when you access the user documentation.