Installing the FX Supervisory Software - Facility Explorer - LIT-12012253 - Server - FX Alarm Portal - FX Workbench - FX Server - 14.x

FX Supervisory Controller Family Software Products Release 14.x Installation Guide

Product
Building Automation Systems > Alarm Portals > FX Alarm Portal
Building Automation Systems > Graphics and Interfaces > FX Workbench
Building Automation Systems > Application Servers > FX Server
Document number
LIT-12012253
Version
14.x
Revision date
2023-03-07

Procedure

  1. Close all applications on the host computer.
  2. Unzip the FX Supervisory Software release file downloaded from the ProFX User Community.
  3. Browse to the location of the software product you intend to install.
    Figure 1. Choose Setup for 64-bit Host

  4. Double-click the appropriate installer for the operating system you are installing on. The FX Supervisory Software Installation window appears.
  5. Click Next to begin installing the software.
  6. Select Yes to accept the license agreement.
  7. Click Next.
  8. Specify the destination folder.
    Note: By default, the destination folder is C:JCI\FXWorkbench-X.X (C:JCI\FXServer-X.X for FX Server installations). You may specify a different destination folder or drive for installation. However, we recommend that you use the default destination folder.

    To specify a different destination folder or drive, click Browse. If you specify a different destination folder, click Refresh to update the Space Available data. The Space Available field displays the drive space available for the installation files.

  9. Select the This instance of Workbench will be used as an installation tool and Install Documentation check boxes.
  10. Click Next.
  11. If you specified a folder that does not exist, a warning dialog box appears.
    Click Yes to create the folder and to continue with the installation process. The Select Options window appears.
  12. Keep the default options and click Next. When the FX Workbench installation is complete, the Finish Install window appears.
  13. To launch FX Workbench upon clicking Finish, select the Launch Workbench check box.
  14. To install and start the platform daemon, select the Install and Start Platform Daemon check box.
  15. Click Finish.

    When the installation is complete, the Niagara platform daemon installs and starts automatically. The Niagara platform daemon is required to support the operation of a station and acts as a server for the platform connections (from the computers running the FX Workbench client).

    If a prior installation of FX Supervisory software exists on the same computer, a window prompts you to restart the platform daemon.

    Figure 2. Platform Daemon Restart Window

  16. Click Continue.
  17. Restart the platform daemon from the Start Menu shortcut.