Input and output terminal blocks - Facility Explorer - Part No. 24-10144-173 - FX-PCX2721-0 - Field Device - FX-PCX27 Expansion Input/Output Module

FX-PCX2721 Expansion Input/Output Module Installation Instructions

Product
Controls > Input/Output Controls > FX-PCX27 Expansion Input/Output Module
Document type
Installation Guide
Document number
Part No. 24-10144-173
Document revision
G
Revision date
2019-03-22

The input terminal blocks are mounted on the bottom of the expansion module and the output terminal blocks are mounted on the top of the expansion module. See Table 1 for more information about I/O terminal functions, requirements, and ratings.