About this task
FX-PCX expansion modules are master devices on MS/TP (SA or FC) buses. Before operating expansion modules on a bus, you must set a valid and unique device address for each expansion module on the bus. You set an expansion module's device address by setting the positions of the switches on the DIP switch block at the top of the expansion module. Device addresses 4 through 127 are the valid addresses for these expansion modules.
The following table describes the FC bus and SA bus device addresses for Johnson Controls MS/TP communications bus applications:
| Device address | Use on description |
|---|---|
|
0 (Switch 128 Off) |
Reserved for FC Bus Supervisory Controller (not for use on controllers or expansion modules). |
|
1 to 3 (Switch 128 Off) |
Reserved for peripheral devices (not for use on controllers or expansion modules). |
|
4 to 127 (Switch 128 Off) |
Used for MS/TP master devices (controllers or expansion modules) that are hardwired to an SA Bus or FC Bus. |
The DIP switch block has eight switches numbered 128, 64, 32, 16, 8, 4, 2, and 1. Switches 64 through 1 are device address switches. Switch 128 is a mode switch that enables an expansion module to operate on an FX-ZFR/ZFR Pro Series Wireless Field Bus. Switch 128 must be set to off for all hard-wired SA and FC bus applications. Set switch 128 to ON for wireless FC bus applications only.
To set the device addresses on FX-PCX expansion modules, complete the following steps: