About this task
Important: Electrostatic discharge can damage expansion module components. Use proper electrostatic discharge precautions during installation, setup, and servicing to avoid damaging the expansion module.
Important: Disconnect all power sources to the expansion module before removing cover and changing the position of any jumper or the EOL switch on the expansion module. Failure to disconnect power before changing a jumper or EOL switch position can result in damage to the expansion module and void any warranties.
The expansion module cover is held in place by four plastic latches that extend from the base and snap into slots on the inside of the housing cover.
To remove the expansion module cover, complete the following steps: