Mounting features and dimensions - Facility Explorer - Part No. 24-10144-173 - FX-PCX2721-0 - Field Device - FX-PCX27 Expansion Input/Output Module

FX-PCX2721 Expansion Input/Output Module Installation Instructions

Product
Controls > Input/Output Controls > FX-PCX27 Expansion Input/Output Module
Document type
Installation Guide
Document number
Part No. 24-10144-173
Document revision
G
Revision date
2019-03-22

See the following figure for mounting dimensions listed in millimeters and inches. Inches are listed in parenthesis. The following figure also illustrates the DIN rail channel and the mounting clips in an extended position.

Figure 1. Back of expansion module