Installation - Facility Explorer - Part No. 24-10144-173 - FX-PCX2721-0 - Field Device - FX-PCX27 Expansion Input/Output Module

FX-PCX2721 Expansion Input/Output Module Installation Instructions

Product
Controls > Input/Output Controls > FX-PCX27 Expansion Input/Output Module
Document type
Installation Guide
Document number
Part No. 24-10144-173
Document revision
G
Revision date
2019-03-22

Observe these guidelines when installing an expansion module:

  • To minimize vibration and shock damage, transport the expansion module in the original container.

  • Verify that all parts shipped with the expansion module.

  • Do not drop the expansion module or subject it to physical shock.