Commissioning - Facility Explorer - Part No. 24-10144-173 - FX-PCX2721-0 - Field Device - FX-PCX27 Expansion Input/Output Module

FX-PCX2721 Expansion Input/Output Module Installation Instructions

Product
Controls > Input/Output Controls > FX-PCX27 Expansion Input/Output Module
Document type
Installation Guide
Document number
Part No. 24-10144-173
Document revision
G
Revision date
2019-03-22

You commission controllers with Controller Configuration Tool (CCT) software, either via a Bluetooth Wireless Commissioning Converter, a ZigBee® wireless dongle, or in BACnet Router mode when connected to Supervisory Controller. Refer to the Controller Tool Help (LIT-12011147) for detailed information on commissioning controllers.

Note: The MAP Gateway serves as a replacement for the BTCVT, which is no longer available for purchase, but continues to be supported.