Application - Facility Explorer - Part No. 24-10144-173 - FX-PCX2721-0 - Field Device - FX-PCX27 Expansion Input/Output Module

FX-PCX2721 Expansion Input/Output Module Installation Instructions

Product
Controls > Input/Output Controls > FX-PCX27 Expansion Input/Output Module
Document number
Part No. 24-10144-173
Document revision
G
Revision date
2019-03-22

The FX-PCX2721 expansion module is part of the Facility Explorer® FX-PC Series Programmable Controller family. FX-PCXs expand the number of Input/Output points connected to either an FX-PCA, FX-PCG, or FX-PCV programmable controller or to a supervisory controller to monitor and control a wide variety of HVAC equipment.

FX-PCXs operate on an RS-485 BACnet® MS/TP Bus and integrate into Johnson Controls® and third-party BACnet systems. FX-PCXs communicate using the BACnet MS/TP protocol when directly connected to the FC Bus.

Note: With Release 10.1 or later of the Controller Configuration Tool (CCT), PCAs, PCGs, or PCVs can be configured to communicate using either the BACnet MS/TP or the N2 field bus networking protocol. The operation of the FX-PCX is not affected by the selection of the BACnet MS/TP or the N2 protocol in the host controller, when the PCX is connected to the host controller using the SA bus.