CAUTION:
CAUTION:
CAUTION:
CAUTION:
Important: Do not exceed the controller electrical ratings. Exceeding
controller electrical ratings can result in permanent damage to the controller and
void any warranty.
Important: Use copper conductors only. Make all wiring in accordance with
local, national, and regional regulations.
Important: Electrostatic discharge can damage controller components. Use
proper electrostatic discharge precautions during installation, setup, and servicing
to avoid damaging the controller.
For detailed information about configuring and wiring an MS/TP bus, FC bus and SA bus, refer to the FX-PC Series Controllers MS/TP Communications Bus Technical Bulletin (LIT-12011670).