Maximum cable length versus load current - Facility Explorer - Part No. 24-10143-616 - Field Device - PCA: Advanced Application Programmable Controller

FX-PCA3611 Advanced Application Programmable Controller Installation Instructions

Product
Controls > Programmable Controls > PCA: Advanced Application Programmable Controller
Document number
Part No. 24-10143-616
Document revision
D
Revision date
2019-03-22

Use Figure 1 to estimate the maximum cable length relative to the wire size and the load current (in mA) when wiring inputs and outputs.

Note: Figure 1 applies to low-voltage (<30 V) inputs and outputs only.
Figure 1. Maximum wire length for low-voltage (<30 V) Inputs and Outputs by current and wire size