Input and Output terminal blocks - Facility Explorer - Part No. 24-10143-616 - Field Device - PCA: Advanced Application Programmable Controller

FX-PCA3611 Advanced Application Programmable Controller Installation Instructions

Product
Controls > Programmable Controls > PCA: Advanced Application Programmable Controller
Document number
Part No. 24-10143-616
Document revision
D
Revision date
2019-03-22

The fixed input terminal blocks are located on the bottom of the controller, and the output terminal blocks are located on the top of the controller. See Table 1 for more information about I/O terminal functions, requirements, and ratings.