The FC bus port on the front of the controller is an RJ-12, 6-position modular jack that provides a connection for the Mobile Access Portal (MAP) Gateway, the FX-BTCVT Bluetooth® Commissioning Converter, or the FX-ZFR/ZFR Pro Wireless Field Bus Router.
The FC bus port is connected internally to the FC bus terminal block. For more information about the FC Bus port functions, requirements, and ratings, see Table 1. The FC bus port pin assignment is shown in Figure 1.
Note:
- The MAP Gateway serves as a replacement for the BTCVT, which is no longer available for purchase, but continues to be supported.
Figure 1. Pin number assignments for sensor, SA bus, and FC bus ports on Controllers