Terminal blocks and bus ports - Facility Explorer - Part No. 24-10143-616 - Field Device - PCA: Advanced Application Programmable Controller

FX-PCA3611 Advanced Application Programmable Controller Installation Instructions

Product
Controls > Programmable Controls > PCA: Advanced Application Programmable Controller
Document type
Installation Guide
Document number
Part No. 24-10143-616
Document revision
D
Revision date
2019-03-22

See FX-PCA3611 physical features for terminal block and bus port locations on the FX-PCA3611 controller. Observe the following guidelines when wiring an FX-PCA3611 controller.