About this task
Each controller has an EOL switch, which, when set to ON, sets the controller as a terminating device on the bus. See Figure 1 for the EOL switch location. The default EOL switch position is Off.
Figure 1. End-of-Line switch positions

To set the EOL switch on an FX-PCA3611 controller, complete the following steps: