Commissioning the Controllers - Facility Explorer - Part No. 24-10143-616 - Field Device - PCA: Advanced Application Programmable Controller

FX-PCA3611 Advanced Application Programmable Controller Installation Instructions

Product
Controls > Programmable Controls > PCA: Advanced Application Programmable Controller
Document number
Part No. 24-10143-616
Document revision
D
Revision date
2019-03-22

You commission BACnet MS/TP controllers with the CCT software, either via a Bluetooth® Wireless Commissioning Converter, a ZFR wireless dongle, or in BACnet router mode when connected to an Supervisory Controller. Refer to Controller Tool Help (LIT-12011147) for detailed information on commissioning controllers.

Note: The MAP Gateway serves as a replacement for the BTCVT, which is no longer available for purchase, but continues to be supported.