DIN rail mount applications - Facility Explorer - Part No. 24-10143-616 - Field Device - PCA: Advanced Application Programmable Controller

FX-PCA3611 Advanced Application Programmable Controller Installation Instructions

Product
Controls > Programmable Controls > PCA: Advanced Application Programmable Controller
Document type
Installation Guide
Document number
Part No. 24-10143-616
Document revision
D
Revision date
2019-03-22

About this task

Mounting the FX-PCA3611 controller horizontally on 35 mm DIN rail is the preferred mounting method.

To mount a controller on 35 mm DIN rail, complete the following steps:

Procedure

  1. Securely mount a 23 cm (9.125 in.) or longer section of 35 mm DIN rail, horizontally and centered in the desired space, so that the controller mounts in the position shown in Figure 1.
  2. Pull the two bottom mounting clips outward from the controller to the extended position (Figure 1).
  3. Hang the controller on the DIN rail by the hooks at the top of the (DIN rail) channel on the back of the controller (Figure 1), and position the controller snugly against the DIN rail.
  4. Push the bottom mounting clips inward (up) to secure the controller on the DIN rail.

    To remove the controller from the DIN rail, pull the bottom mounting clips out to the extended position and carefully lift the controller off the DIN rail.